Keysight 89600 VSA .NET API
CyclicPrefixLengthModeType Enumeration
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : CyclicPrefixLengthModeType Enumeration


Glossary Item Box

Specifies the Cyclic-prefix length mode.

Syntax

Visual Basic (Declaration) 
Public Enum CyclicPrefixLengthModeType 
   Inherits System.Enum
C# 
public enum CyclicPrefixLengthModeType : System.Enum 
C++/CLI 
public enum class CyclicPrefixLengthModeType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AutoAuto-detect the CP length mode.—
ExtendedCP Length mode is Extended.—
NormalCP Length mode is Normal.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also