Keysight 89600 VSA .NET API
DuplexModeType Enumeration
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : DuplexModeType Enumeration


Glossary Item Box

Specifies the duplex mode: FDD or TDD

Syntax

Visual Basic (Declaration) 
Public Enum DuplexModeType 
   Inherits System.Enum
C# 
public enum DuplexModeType : System.Enum 
C++/CLI 
public enum class DuplexModeType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
FddDuplex mode is FDD.—
TddDuplex mode is TDD.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also