Keysight 89600 VSA .NET API
EvmMinimizationType Enumeration
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : EvmMinimizationType Enumeration


Glossary Item Box

Specifies the EVM Minimization method to use.

Syntax

Visual Basic (Declaration) 
Public Enum EvmMinimizationType 
   Inherits System.Enum
C# 
public enum EvmMinimizationType : System.Enum 
C++/CLI 
public enum class EvmMinimizationType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
LowSnrEVM Minimization is based on 3GPP non-compliant pilot tracking procedure, using synchronization algorithms optimized for low SNR (Signal to Noise Ratio) test scenarios. The LowSnr selection is currently only available when MeasurementExtension.LinkDirection is LinkDirectionType.Uplink.29.40
OffEVM Minimization is off.—
ThreeGppEVM Minimization is based on the 3GPP-defined procedure.—
TrackingEVM Minimization is based on 3GPP non-compliant pilot tracking procedure.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also