Keysight 89600 VSA .NET API
InputChannelType Enumeration
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : InputChannelType Enumeration


Glossary Item Box

Specifies the measurement input channel.

Syntax

Visual Basic (Declaration) 
Public Enum InputChannelType 
   Inherits System.Enum
C# 
public enum InputChannelType : System.Enum 
C++/CLI 
public enum class InputChannelType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
Channel1Measurement input channel is Channel 1.—
Channel10Measurement input channel is Channel 2.—
Channel11Measurement input channel is Channel 3.—
Channel12Measurement input channel is Channel 4.—
Channel13Measurement input channel is Channel 5.15.00
Channel14Measurement input channel is Channel 6.15.00
Channel15Measurement input channel is Channel 7.15.00
Channel16Measurement input channel is Channel 8.15.00
Channel17Measurement input channel is Channel 1.—
Channel18Measurement input channel is Channel 2.—
Channel19Measurement input channel is Channel 3.—
Channel2Measurement input channel is Channel 2.—
Channel20Measurement input channel is Channel 4.—
Channel21Measurement input channel is Channel 5.15.00
Channel22Measurement input channel is Channel 6.15.00
Channel23Measurement input channel is Channel 7.15.00
Channel24Measurement input channel is Channel 8.15.00
Channel25Measurement input channel is Channel 1.—
Channel26Measurement input channel is Channel 2.—
Channel27Measurement input channel is Channel 3.—
Channel28Measurement input channel is Channel 4.—
Channel29Measurement input channel is Channel 5.15.00
Channel3Measurement input channel is Channel 3.—
Channel30Measurement input channel is Channel 6.15.00
Channel31Measurement input channel is Channel 7.15.00
Channel32Measurement input channel is Channel 8.15.00
Channel33Measurement input channel is Channel 1.—
Channel34Measurement input channel is Channel 2.—
Channel35Measurement input channel is Channel 3.—
Channel36Measurement input channel is Channel 4.—
Channel37Measurement input channel is Channel 5.15.00
Channel38Measurement input channel is Channel 6.15.00
Channel39Measurement input channel is Channel 7.15.00
Channel4Measurement input channel is Channel 4.—
Channel40Measurement input channel is Channel 8.15.00
Channel41Measurement input channel is Channel 1.—
Channel42Measurement input channel is Channel 2.—
Channel43Measurement input channel is Channel 3.—
Channel44Measurement input channel is Channel 4.—
Channel45Measurement input channel is Channel 5.15.00
Channel46Measurement input channel is Channel 6.15.00
Channel47Measurement input channel is Channel 7.15.00
Channel48Measurement input channel is Channel 8.15.00
Channel49Measurement input channel is Channel 1.—
Channel5Measurement input channel is Channel 5.15.00
Channel50Measurement input channel is Channel 2.—
Channel51Measurement input channel is Channel 3.—
Channel52Measurement input channel is Channel 4.—
Channel53Measurement input channel is Channel 5.15.00
Channel54Measurement input channel is Channel 6.15.00
Channel55Measurement input channel is Channel 7.15.00
Channel56Measurement input channel is Channel 8.15.00
Channel57Measurement input channel is Channel 1.—
Channel58Measurement input channel is Channel 2.—
Channel59Measurement input channel is Channel 3.—
Channel6Measurement input channel is Channel 6.15.00
Channel60Measurement input channel is Channel 4.—
Channel61Measurement input channel is Channel 5.15.00
Channel62Measurement input channel is Channel 6.15.00
Channel63Measurement input channel is Channel 7.15.00
Channel64Measurement input channel is Channel 8.15.00
Channel7Measurement input channel is Channel 7.15.00
Channel8Measurement input channel is Channel 8.15.00
Channel9Measurement input channel is Channel 1.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Remarks

Used to indicate the reference measurement input channel.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also