Keysight 89600 VSA .NET API
Create Method
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > LayerCollection Class : Create Method


Glossary Item Box

Creates a new LTE Layer.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function Create() As Layer
C# 
public abstract Layer Create()
C++/CLI 
public:
abstract Layer^ Create(); 

Return Value

A handle to the new Layer.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also