Keysight 89600 VSA .NET API
ModulationFormatType Enumeration
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : ModulationFormatType Enumeration


Glossary Item Box

Specifies the modulation format used by data channels.

Syntax

Visual Basic (Declaration) 
Public Enum ModulationFormatType 
   Inherits System.Enum
C# 
public enum ModulationFormatType : System.Enum 
C++/CLI 
public enum class ModulationFormatType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
Qam1024modulation format is 1024-QAM24.00
Qam16modulation format is 16-QAM.—
Qam256modulation format is 256-QAM20.00
Qam64modulation format is 64-QAM.—
Qpskmodulation format is QPSK.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also