Keysight 89600 VSA .NET API
NumberOfCsiRsPortsType Enumeration
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : NumberOfCsiRsPortsType Enumeration


Glossary Item Box

Specifies the number of CSI-RS ports

Syntax

Visual Basic (Declaration) 
Public Enum NumberOfCsiRsPortsType 
   Inherits System.Enum
C# 
public enum NumberOfCsiRsPortsType : System.Enum 
C++/CLI 
public enum class NumberOfCsiRsPortsType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
EightEight CSI-RS Ports—
FourFour CSI-RS Ports—
OneOne CSI-RS Port—
TwoTwo CSI-RS Ports—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 16.00

See Also