Keysight 89600 VSA .NET API
NumberOfLayersType Enumeration
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : NumberOfLayersType Enumeration


Glossary Item Box

Specifies the Number of Layers to be decoded from Spatial Multiplexed DL Shared Channels (PDSCH)

Syntax

Visual Basic (Declaration) 
Public Enum NumberOfLayersType 
   Inherits System.Enum
C# 
public enum NumberOfLayersType : System.Enum 
C++/CLI 
public enum class NumberOfLayersType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
FourFour layers to be decoded.—
OneOne layer to be decoded.—
ThreeThree layers to be decoded.—
TwoTwo layers to be decoded.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also