Keysight 89600 VSA .NET API
NumberOfTXAntennasType Enumeration
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : NumberOfTXAntennasType Enumeration


Glossary Item Box

Specifies the total number of tx antenna ports for currently configured transmission system (Downlink only).

Syntax

Visual Basic (Declaration) 
Public Enum NumberOfTXAntennasType 
   Inherits System.Enum
C# 
public enum NumberOfTXAntennasType : System.Enum 
C++/CLI 
public enum class NumberOfTXAntennasType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
FourTransmission system configured for 4 Antenna ports in total.—
OneTransmission system configured for 1 Antenna port in total.—
TwoTransmission system configured for 2 Antenna ports in total.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also