Keysight 89600 VSA .NET API
OrthogonalCoverCodeType Enumeration
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : OrthogonalCoverCodeType Enumeration


Glossary Item Box

Specifies the Orthogonal Cover Code used by the PUSCH DMRS sequence

Syntax

Visual Basic (Declaration) 
Public Enum OrthogonalCoverCodeType 
   Inherits System.Enum
C# 
public enum OrthogonalCoverCodeType : System.Enum 
C++/CLI 
public enum class OrthogonalCoverCodeType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
PlusOneMinusOneOCC for slots 0 and 1 is [1 -1]—
PlusOnePlusOneOCC for slots 0 and 1 is [1 1]—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 18.0

See Also