Keysight 89600 VSA .NET API
PdschCellSpecificRatioType Enumeration
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : PdschCellSpecificRatioType Enumeration


Glossary Item Box

Specifies the PDSCH Cell Specific Ratio p_B/p_A

Syntax

Visual Basic (Declaration) 
Public Enum PdschCellSpecificRatioType 
   Inherits System.Enum
C# 
public enum PdschCellSpecificRatioType : System.Enum 
C++/CLI 
public enum class PdschCellSpecificRatioType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
Oneuse fixed p_B/p_A ratio = 1.0.—
PB0use cell specific ratio parameter P_B = 0.—
PB1use cell specific ratio parameter P_B = 1.—
PB2use cell specific ratio parameter P_B = 2.—
PB3use cell specific ratio parameter P_B = 3.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also