Keysight 89600 VSA .NET API
PuschBitVectorSelectType Enumeration
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : PuschBitVectorSelectType Enumeration


Glossary Item Box

Specifies the PUSCH Bit Vector Selection which determines PUSCH bit values are displayed in Decoded Symbol Table trace

Syntax

Visual Basic (Declaration) 
Public Enum PuschBitVectorSelectType 
   Inherits System.Enum
C# 
public enum PuschBitVectorSelectType : System.Enum 
C++/CLI 
public enum class PuschBitVectorSelectType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
DecodedCBDecoded Symbol Table trace displays PUSCH decoded code block bit values.—
DecodedTBDecoded Symbol Table trace displays PUSCH decoded transport block bit values.—
DeRateMatchedDecoded Symbol Table trace displays PUSCH de-rate-matched bit values.—
DescrambledDecoded Symbol Table trace displays PUSCH descrambled bit values.—
MappedDecoded Symbol Table trace does not display PUSCH bit values.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also