Keysight 89600 VSA .NET API
PuxchTddAckNackFeedbackModeType Enumeration
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : PuxchTddAckNackFeedbackModeType Enumeration


Glossary Item Box

Specifies the PUSCH/PUCCH TDD Ack/Nack Feedback Mode used by VSA to decode PUSCH and PUCCH HARQ Ack/Nack bits.

Syntax

Visual Basic (Declaration) 
Public Enum PuxchTddAckNackFeedbackModeType 
   Inherits System.Enum
C# 
public enum PuxchTddAckNackFeedbackModeType : System.Enum 
C++/CLI 
public enum class PuxchTddAckNackFeedbackModeType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
BundlingVSA Decodes TDD mode PUSCH/PUCCH HARQ bits as per 3GPP Ack/Nack Feedback Mode = Bundling definition.—
MultiplexingVSA Decodes TDD mode PUSCH/PUCCH HARQ bits as per 3GPP Ack/Nack Feedback Mode = Multiplexing definition.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also