Keysight 89600 VSA .NET API
RateMatchPatternSlotPatternPeriodicity Enumeration
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : RateMatchPatternSlotPatternPeriodicity Enumeration


Glossary Item Box

Enum value indicating the length of the slot-pattern repetition window over which the slot-pattern bitmap applies.

Syntax

Visual Basic (Declaration) 
Public Enum RateMatchPatternSlotPatternPeriodicity 
   Inherits System.Enum
C# 
public enum RateMatchPatternSlotPatternPeriodicity : System.Enum 
C++/CLI 
public enum class RateMatchPatternSlotPatternPeriodicity : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
EightThe size of the slot-pattern bitmap is 8 (N8). The cycle spans 8 slots (4 ms).—
FiveThe size of the slot-pattern bitmap is 5 (N5). The cycle spans 5 slots (2.5 ms).—
FourThe size of the slot-pattern bitmap is 4 (N4). The cycle spans 4 slots (2 ms).—
OneThe size of the slot-pattern bitmap is 1 (N1). The re-mask is evaluated every slot.—
TenThe size of the slot-pattern bitmap is 10 (N10). The cycle spans 10 slots (5 ms).—
TwentyThe size of the slot-pattern bitmap is 20 (N20). The cycle spans 20 slots = 10 ms (one full LTE radio frame).—
TwoThe size of the slot-pattern bitmap is 2 (N2). The cycle spans 2 slots (1 ms).—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Remarks

One LTE slot is 0.5 ms in duration and contains 7 OFDM symbols with normal cyclic prefix or 6 OFDM symbols with extended cyclic prefix.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 31.00

See Also