Keysight 89600 VSA .NET API
SpecialSubframeConfigurationType Enumeration
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : SpecialSubframeConfigurationType Enumeration


Glossary Item Box

Specifies the Dw/GP/Up Length for TDD.

Syntax

Visual Basic (Declaration) 
Public Enum SpecialSubframeConfigurationType 
   Inherits System.Enum
C# 
public enum SpecialSubframeConfigurationType : System.Enum 
C++/CLI 
public enum class SpecialSubframeConfigurationType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
Configuration0Special subframe configuration 0.—
Configuration1Special subframe configuration 1.—
Configuration2Special subframe configuration 2.—
Configuration3Special subframe configuration 3.—
Configuration4Special subframe configuration 4.—
Configuration5Special subframe configuration 5.—
Configuration6Special subframe configuration 6.—
Configuration7Special subframe configuration 7.—
Configuration8Special subframe configuration 8.—
Configuration9Special subframe configuration 9.18.00
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Remarks

Applies only to TDD.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also