Keysight 89600 VSA .NET API
SynchronizationSignalPrecodingType Enumeration
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : SynchronizationSignalPrecodingType Enumeration


Glossary Item Box

Specifies if the sync signals have precoding applied.

Syntax

Visual Basic (Declaration) 
Public Enum SynchronizationSignalPrecodingType 
   Inherits System.Enum
C# 
public enum SynchronizationSignalPrecodingType : System.Enum 
C++/CLI 
public enum class SynchronizationSignalPrecodingType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
OffSync signals Precoding = Off—
OnSync signals Precoding = On—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 20.00

See Also