Keysight 89600 VSA .NET API
TransmissionModeTypes Enumeration
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : TransmissionModeTypes Enumeration


Glossary Item Box

Specifies which Transmission Modes are included, so that decoding of the appropriate DCI Format may be attempted.

Syntax

Visual Basic (Declaration) 
Public Enum TransmissionModeTypes 
   Inherits System.Enum
C# 
public enum TransmissionModeTypes : System.Enum 
C++/CLI 
public enum class TransmissionModeTypes : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
NoneTransmission Mode 119.00
TM1Transmission Mode 119.00
TM2Transmission Mode 219.00
TM3Transmission Mode 319.00
TM4Transmission Mode 419.00
TM5Transmission Mode 519.00
TM6Transmission Mode 619.00
TM7Transmission Mode 719.00
TM8Transmission Mode 819.00
TM9Transmission Mode 919.00
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also