Keysight 89600 VSA .NET API
UplinkUserCollection Class
Members  See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : UplinkUserCollection Class


Glossary Item Box

The Lte.UplinkUserCollection class contains properties and methods to manipulate a collection of LTE UplinkUser objects.

Object Model

UplinkUserCollection ClassUplinkUser ClassPrach ClassAllocationCollection ClassPucch ClassAllocationCollection ClassPusch ClassAllocationCollection ClassSrs ClassAllocationCollection ClassUplinkUser ClassPrach ClassAllocationCollection ClassPucch ClassAllocationCollection ClassPusch ClassAllocationCollection ClassSrs ClassAllocationCollection Class

Syntax

Visual Basic (Declaration) 
Public MustInherit Class UplinkUserCollection 
   Inherits Agilent.SA.Vsa.Lte.UserCollection(Of UplinkUser)
   Implements Agilent.SA.Vsa.ICollectionBase, Agilent.SA.Vsa.ICollectionBase(Of UplinkUser), Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyCollectionChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3 

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also