Keysight 89600 VSA .NET API
RmsEvm Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Keysight.SA.Vsa.ContextExtensions.Lte Namespace > CalculationResult Class : RmsEvm Property


Glossary Item Box

Gets the rms evm result with unit of percent(%).

Syntax

Visual Basic (Declaration) 
Public ReadOnly Property RmsEvm As Double
C# 
public double RmsEvm {get;}
C++/CLI 
public:
property double RmsEvm {
   double get();
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also