Keysight 89600 VSA .NET API
TotalCodeBlockCount Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Keysight.SA.Vsa.ContextExtensions.Lte Namespace > CalculationResult Class : TotalCodeBlockCount Property


Glossary Item Box

Gets the total code block count result with unit of code blocks. The number of transport data code blocks measured for BLER test.

Syntax

Visual Basic (Declaration) 
Public ReadOnly Property TotalCodeBlockCount As Long
C# 
public long TotalCodeBlockCount {get;}
C++/CLI 
public:
property int64 TotalCodeBlockCount {
   int64 get();
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also