Keysight 89600 VSA .NET API
ConfigureWithVsaSetupFile Method
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Keysight.SA.Vsa.ContextExtensions.Lte Namespace > LteDirectCalculation Class : ConfigureWithVsaSetupFile Method


fileName
The VSA setx file name with full path
calculationControl
The control for this calculation

Glossary Item Box

Configures this DirectCalculation with VSA setx file.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function ConfigureWithVsaSetupFile( _
   ByVal fileName As String, _
   ByVal calculationControl As CalculationControl _
) As ConfigurationResult
C# 
public abstract ConfigurationResult ConfigureWithVsaSetupFile( 
   string fileName,
   CalculationControl calculationControl
)
C++/CLI 
public:
abstract ConfigurationResult^ ConfigureWithVsaSetupFile( 
   String^ fileName,
   CalculationControl^ calculationControl
) 

Parameters

fileName
The VSA setx file name with full path
calculationControl
The control for this calculation

Return Value

ConfigurationResult is returned which includes the overall status, all the status messages, the signal format, and all the requirements for the input data.

Remarks

When the measurement extension defined in the setx file is not LTE, Keysight.SA.Vsa.OverallStatus.Error will be returned in ConfigurationResult.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also