Keysight 89600 VSA .NET API
WaitForCalculationDone Method
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Keysight.SA.Vsa.ContextExtensions.Lte Namespace > LteDirectCalculation Class : WaitForCalculationDone Method


millisecondsTimeout
The number of milliseconds to wait.

Glossary Item Box

Waits for the calculation to complete.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function WaitForCalculationDone( _
   ByVal millisecondsTimeout As Integer _
) As Boolean
C# 
public abstract bool WaitForCalculationDone( 
   int millisecondsTimeout
)
C++/CLI 
public:
abstract bool WaitForCalculationDone( 
   int millisecondsTimeout
) 

Parameters

millisecondsTimeout
The number of milliseconds to wait.

Return Value

A value indicating whether the calculation is complete

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also