Keysight 89600 VSA .NET API
Mcs Property
See Also 
Agilent.SA.Vsa.NBIot.Interfaces Assembly > Agilent.SA.Vsa.NBIot Namespace > DownlinkUser Class : Mcs Property


Glossary Item Box

Gets or sets the MCS (modulation and coding scheme).

Syntax

Visual Basic (Declaration) 
Public MustOverride Property Mcs As Integer
C# 
public abstract int Mcs {get; set;}
C++/CLI 
public:
abstract property int Mcs {
   int get();
   void set (    int value);
}

Property Value

The default value is 0.

Remarks

When MeasurementExtension.RBAutoDetectMode = RBAutoDetectModeType.Off (manual allocation) multiple defined NPDSCH users can be decoded. When = RBAutoDetectModeType.PowerBased a single auto-detected NPDSCH user can be decoded.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also