| Class | Description | |
|---|---|---|
![]() | Channel | The Channel class contains properties and methods that are common to a NB-IoT channel. |
![]() | DownlinkUser | The DownlinkUser class contains properties and methods specific to NB-IoT Downlink users. |
![]() | DownlinkUserCollection | The DownlinkUserCollection class contains properties and methods to manipulate a collection of NB-IoT DownlinkUser objects. |
![]() | MeasurementExtension | The MeasurementExtension class contains properties and methods to control NB-IoT demodulation. |
![]() | Nprach | The Nprach class contains properties and methods to control the behavior of NPRACH channel. |
![]() | Npusch | The Npusch class contains properties and methods to control the behavior of NPUSCH channel. |
![]() | UplinkUser | The UplinkUser class contains properties and methods specific to NB-IoT Uplink users. |
![]() | UplinkUserCollection | The UplinkUserCollection class contains properties and methods to manipulate a collection of UplinkUser objects. |
![]() | UserCollection<T> | The UserCollection<T> class contains properties and methods that are common to the manipulation of a collection of users. |
| Enumeration | Description | |
|---|---|---|
![]() | AnalysisBoundaryType | Specifies the analysis start boundary. |
![]() | CellIdModeType | Specifies the Physical-layer Cell Identity Mode. |
![]() | EqualizerTrainingModeType | Specifies the Equalizer Training mode. |
![]() | EqualizerTrainingType | Specifies the Equalizer Training method. |
![]() | EvmMinimizationType | Specifies the EVM Minimization method to use. |
![]() | LayerDecodingType | Specifies what type of decoding to apply to downlink channels. Only applies when MeasurementExtension.NumberOfNrsAntennas > 1. |
![]() | LinkDirectionType | Specifies the link direction. |
![]() | LteTransmissionBandwidthType | Specifies the LTE transmission bandwidth when MeasurementExtension.OperationMode is in-band. |
![]() | NpbchBitVectorSelectType | Specifies the NPBCH bit values to be displayed in Decoded Symbol Table trace. |
![]() | NpdschBitVectorSelectType | Specifies the NPDSCH bit values to be displayed in Decoded Symbol Table trace |
![]() | NpdschNumberOfRepetitionsType | Specifies the number of repetitions for an NPDSCH allocation. |
![]() | NpdschNumberOfSubframesType | Specifies the number of subframes for a NPDSCH allocation. |
![]() | NprachNumberOfRepetitionsType | Specifies the number of repetitions in an NPRACH burst. |
![]() | NprachNumberOfSubcarriersType | Specifies the number of subcarriers in NPRACH. |
![]() | NprachPreambleFormatType | Specifies the NPRACH preamble format. |
![]() | NprachStartTimeType | Specifies the start time (sec) of the NPRACH burst. |
![]() | NprachSubcarrierOffsetType | Specifies the subcarrier offset for NPRACH. |
![]() | NpuschBitVectorSelectType | Specifies the NPUSCH bit values to be displayed in the UL Decoded Symbol Table trace. |
![]() | NpuschFormatType | Specifies the NPUSCH format. |
![]() | NpuschNumberOfRepetitionsType | Specifies the number of repetitions of the NPUSCH signal. |
![]() | NpuschRUNumberType | Number of resource units in NPUSCH. |
![]() | NpuschSubcarrierOffsetType | Specifies the NPUSCH subcarrier offset. |
![]() | NpuschSubcarrierSpacingType | Specifies the NPUSCH subcarrier spacing. |
![]() | NpuschToneNumberType | Specifies the number of tones in NPUSCH. |
![]() | NrsReferenceAntennaPortType | Specifies the antenna port number on which the NRS transmission takes place. |
![]() | NumberOfEutraCrsAntennaPortsType | Specifies the total number of CRS antenna ports when MeasurementExtension.OperationMode is in-band. |
![]() | NumberOfNrsAntennaPortsType | Specifies the total number of NRS antenna ports for currently configured transmission system. |
![]() | OperationModeType | Specifies the NB-IoT operation mode (downlink-only). |
![]() | RBAutoDetectModeType | Specifies the RB Auto Detect Mode which determines the method used to determine what allocations are present. |
![]() | SharedChannelDecoderType | Specifies what type of level of decoding should be applied to NPDSCH. |
![]() | SingleToneModulationFormatType | Specifies the modulation format used by NPUSCH when MeasurementExtension.NpuschToneNumber == NpuschToneNumberType.SingleTone. |
![]() | SubframeChannelType | Specifies the channel expected in a downlink subframe. |
![]() | SymbolTimeAdjustmentMode | Specifies the Symbol Time Adjust method used for EVM measurements. |
![]() | SynchronizationSignalAntennaPortType | Specifies the NPSS/NSSS Antenna Port or Ports used for synchronization signal transmission |
![]() | SynchronizationTypeSelection | Specifies which channel/signal to use for synchronization |
![]() | UplinkOperationModeType | Specifies the NB-IoT operation mode (uplink-only). |