Keysight 89600 VSA .NET API
StartSubframe Property
See Also 
Agilent.SA.Vsa.NBIot.Interfaces Assembly > Agilent.SA.Vsa.NBIot Namespace > DownlinkUser Class : StartSubframe Property


Glossary Item Box

Gets or sets the starting subframe of the NPUSCH transmission.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property StartSubframe As Integer
C# 
public abstract int StartSubframe {get; set;}
C++/CLI 
public:
abstract property int StartSubframe {
   int get();
   void set (    int value);
}

Remarks

When MeasurementExtension.RBAutoDetectMode = RBAutoDetectModeType.Off the start subframe is derived automatically from the user's allocated slots (the first allocated slot) and is read-only. When = RBAutoDetectModeType.PowerBased it is set explicitly. Decoding is supported in both modes.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also