Keysight 89600 VSA .NET API
EvmMinimizationType Enumeration
See Also 
Agilent.SA.Vsa.NBIot.Interfaces Assembly > Agilent.SA.Vsa.NBIot Namespace : EvmMinimizationType Enumeration


Glossary Item Box

Specifies the EVM Minimization method to use.

Syntax

Visual Basic (Declaration) 
Public Enum EvmMinimizationType 
   Inherits System.Enum
C# 
public enum EvmMinimizationType : System.Enum 
C++/CLI 
public enum class EvmMinimizationType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
OffEVM Minimization is off.—
ThreeGppEVM Minimization is based on the 3GPP-defined procedure.—
TrackingEVM Minimization is based on non-3GPP-compliant pilot tracking procedure.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also