Keysight 89600 VSA .NET API
LinkDirectionType Enumeration
See Also 
Agilent.SA.Vsa.NBIot.Interfaces Assembly > Agilent.SA.Vsa.NBIot Namespace : LinkDirectionType Enumeration


Glossary Item Box

Specifies the link direction.

Syntax

Visual Basic (Declaration) 
Public Enum LinkDirectionType 
   Inherits System.Enum
C# 
public enum LinkDirectionType : System.Enum 
C++/CLI 
public enum class LinkDirectionType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
DownlinkDirection is Downlink.—
UplinkDirection is Uplink.24.00
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also