Keysight 89600 VSA .NET API
LteTransmissionBandwidthType Enumeration
See Also 
Agilent.SA.Vsa.NBIot.Interfaces Assembly > Agilent.SA.Vsa.NBIot Namespace : LteTransmissionBandwidthType Enumeration


Glossary Item Box

Specifies the LTE transmission bandwidth when MeasurementExtension.OperationMode is in-band.

Syntax

Visual Basic (Declaration) 
Public Enum LteTransmissionBandwidthType 
   Inherits System.Enum
C# 
public enum LteTransmissionBandwidthType : System.Enum 
C++/CLI 
public enum class LteTransmissionBandwidthType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
BW10Mhz50RBBandwidth is 10 MHz (50 RBs).—
BW15Mhz75RBBandwidth is 15 MHz (75 RBs).—
BW20Mhz100RBBandwidth is 20 MHz (100 RBs).—
BW3Mhz15RBBandwidth is 3 MHz (15 RBs).—
BW5Mhz25RBBandwidth is 5 MHz (25 RBs).—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also