Keysight 89600 VSA .NET API
NpdschNumberOfSubframesType Enumeration
See Also 
Agilent.SA.Vsa.NBIot.Interfaces Assembly > Agilent.SA.Vsa.NBIot Namespace : NpdschNumberOfSubframesType Enumeration


Glossary Item Box

Specifies the number of subframes for a NPDSCH allocation.

Syntax

Visual Basic (Declaration) 
Public Enum NpdschNumberOfSubframesType 
   Inherits System.Enum
C# 
public enum NpdschNumberOfSubframesType : System.Enum 
C++/CLI 
public enum class NpdschNumberOfSubframesType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
N1One resource unit.—
N10Ten resource units.—
N2Two resource units.—
N3Three resource units.—
N4Four resource units.—
N5Five resource units.—
N6Six resource units.—
N8Eight resource units.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also