Keysight 89600 VSA .NET API
NprachStartTimeType Enumeration
See Also 
Agilent.SA.Vsa.NBIot.Interfaces Assembly > Agilent.SA.Vsa.NBIot Namespace : NprachStartTimeType Enumeration


Glossary Item Box

Specifies the start time (sec) of the NPRACH burst.

Syntax

Visual Basic (Declaration) 
Public Enum NprachStartTimeType 
   Inherits System.Enum
C# 
public enum NprachStartTimeType : System.Enum 
C++/CLI 
public enum class NprachStartTimeType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
N10241024 milliseconds—
N128128 milliseconds—
N1616 milliseconds—
N256256 milliseconds—
N3232 milliseconds—
N512512 milliseconds—
N6464 milliseconds—
N88 milliseconds—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also