Keysight 89600 VSA .NET API
NumberOfSubcarriers Property
See Also 
Agilent.SA.Vsa.NBIot.Interfaces Assembly > Agilent.SA.Vsa.NBIot Namespace > Nprach Class : NumberOfSubcarriers Property


Glossary Item Box

Gets or sets the number of NPRACH subcarriers (N_SC).

Syntax

Visual Basic (Declaration) 
Public MustOverride Property NumberOfSubcarriers As NprachNumberOfSubcarriersType
C# 
public abstract NprachNumberOfSubcarriersType NumberOfSubcarriers {get; set;}
C++/CLI 
public:
abstract property NprachNumberOfSubcarriersType NumberOfSubcarriers {
   NprachNumberOfSubcarriersType get();
   void set (    NprachNumberOfSubcarriersType value);
}

Property Value

The default value is NprachNumberOfSubcarriersType.N12.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also