Keysight 89600 VSA .NET API
NpuschBitVectorSelectType Enumeration
See Also 
Agilent.SA.Vsa.NBIot.Interfaces Assembly > Agilent.SA.Vsa.NBIot Namespace : NpuschBitVectorSelectType Enumeration


Glossary Item Box

Specifies the NPUSCH bit values to be displayed in the UL Decoded Symbol Table trace.

Syntax

Visual Basic (Declaration) 
Public Enum NpuschBitVectorSelectType 
   Inherits System.Enum
C# 
public enum NpuschBitVectorSelectType : System.Enum 
C++/CLI 
public enum class NpuschBitVectorSelectType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
DecodedCBDecoded Symbol Table trace displays NPUSCH decoded code block bit values.—
DecodedTBDecoded Symbol Table trace displays NPUSCH decoded transport block bit values.—
DeRateMatchedDecoded Symbol Table trace displays NPUSCH de-rate-matched bit values.—
DescrambledDecoded Symbol Table trace displays NPUSCH descrambled bit values.—
MappedDecoded Symbol Table trace does not display NPUSCH bit values.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also