Keysight 89600 VSA .NET API
Repetitions Property
See Also 
Agilent.SA.Vsa.NBIot.Interfaces Assembly > Agilent.SA.Vsa.NBIot Namespace > Npusch Class : Repetitions Property


Glossary Item Box

Gets or sets the number of repetitions (N_Rep).

Syntax

Visual Basic (Declaration) 
Public MustOverride Property Repetitions As NpuschNumberOfRepetitionsType
C# 
public abstract NpuschNumberOfRepetitionsType Repetitions {get; set;}
C++/CLI 
public:
abstract property NpuschNumberOfRepetitionsType Repetitions {
   NpuschNumberOfRepetitionsType get();
   void set (    NpuschNumberOfRepetitionsType value);
}

Property Value

The default value is NpuschNumberOfRepetitionsType.N1.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also