Keysight 89600 VSA .NET API
NrsReferenceAntennaPortType Enumeration
See Also 
Agilent.SA.Vsa.NBIot.Interfaces Assembly > Agilent.SA.Vsa.NBIot Namespace : NrsReferenceAntennaPortType Enumeration


Glossary Item Box

Specifies the antenna port number on which the NRS transmission takes place.

Syntax

Visual Basic (Declaration) 
Public Enum NrsReferenceAntennaPortType 
   Inherits System.Enum
C# 
public enum NrsReferenceAntennaPortType : System.Enum 
C++/CLI 
public enum class NrsReferenceAntennaPortType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
Port2000Transmission is on Antenna port number 2000.—
Port2001Transmission is on Antenna port number 2001.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also