Keysight 89600 VSA .NET API
NumberOfEutraCrsAntennaPortsType Enumeration
See Also 
Agilent.SA.Vsa.NBIot.Interfaces Assembly > Agilent.SA.Vsa.NBIot Namespace : NumberOfEutraCrsAntennaPortsType Enumeration


Glossary Item Box

Specifies the total number of CRS antenna ports when MeasurementExtension.OperationMode is in-band.

Syntax

Visual Basic (Declaration) 
Public Enum NumberOfEutraCrsAntennaPortsType 
   Inherits System.Enum
C# 
public enum NumberOfEutraCrsAntennaPortsType : System.Enum 
C++/CLI 
public enum class NumberOfEutraCrsAntennaPortsType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
FourFour CRS Antenna ports—
OneOne CRS Antenna port—
TwoTwo CRS Antenna ports—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also