Keysight 89600 VSA .NET API
SynchronizationSignalAntennaPortType Enumeration
See Also 
Agilent.SA.Vsa.NBIot.Interfaces Assembly > Agilent.SA.Vsa.NBIot Namespace : SynchronizationSignalAntennaPortType Enumeration


Glossary Item Box

Specifies the NPSS/NSSS Antenna Port or Ports used for synchronization signal transmission

Syntax

Visual Basic (Declaration) 
Public Enum SynchronizationSignalAntennaPortType 
   Inherits System.Enum
C# 
public enum SynchronizationSignalAntennaPortType : System.Enum 
C++/CLI 
public enum class SynchronizationSignalAntennaPortType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AllPortsNPSS/NSSS transmitted on all Antenna Ports.—
Port2000NPSS/NSSS transmitted on Antenna Port 2000 only.—
Port2001NPSS/NSSS transmitted on Antenna Port 2001 only.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also