Keysight 89600 VSA .NET API
IsCarrierEnabled Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > CarrierMapping Class : IsCarrierEnabled Property


Glossary Item Box

Gets or sets a value indicating whether the carrier mapping is marked as enabled.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsCarrierEnabled As Boolean
C# 
public abstract bool IsCarrierEnabled {get; set;}
C++/CLI 
public:
abstract property bool IsCarrierEnabled {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also