Keysight 89600 VSA .NET API
IsPhaseContiguousAcrossSlots Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > CarrierMapping Class : IsPhaseContiguousAcrossSlots Property


Glossary Item Box

Gets or sets a value indicating whether the phase across slots is contiguous or not on this carrier.

Syntax

Visual Basic (Declaration) 
Public Overridable Property IsPhaseContiguousAcrossSlots As Boolean
C# 
public virtual bool IsPhaseContiguousAcrossSlots {get; set;}
C++/CLI 
public:
virtual property bool IsPhaseContiguousAcrossSlots {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Remarks

This value affects the phase tracking algorithm. When true, the phase tracking algorithm assumes that the LO phase is contiguous across the slots. When false, the phase tracking algorithm assumes that the LO phase is noncontiguous across the slots.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 28.40

See Also