Gets or sets a value indicating the first slot index of the repetition pattern.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property SignalRepetitionFirstSlotIndex As Integer |
| C# | |
|---|
public virtual int SignalRepetitionFirstSlotIndex {get; set;} |
| C++/CLI | |
|---|
public:
virtual property int SignalRepetitionFirstSlotIndex {
int get();
void set ( int value);
} |
Property Value
The default value is 0.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 27.40
See Also