Keysight 89600 VSA .NET API
UplinkFrequencyHigh Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > CarrierMapping Class : UplinkFrequencyHigh Property


Glossary Item Box

Gets or sets the absolute high end of operation band in hertz of this carrier mapping for Uplink.

Syntax

Visual Basic (Declaration) 
Public Overridable Property UplinkFrequencyHigh As Double
C# 
public virtual double UplinkFrequencyHigh {get; set;}
C++/CLI 
public:
virtual property double UplinkFrequencyHigh {
   double get();
   void set (    double value);
}

Property Value

The default value is 1GHz.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also