Gets or sets the absolute Low end of operation band in hertz of this carrier mapping for Uplink.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property UplinkFrequencyLow As Double |
| C# | |
|---|
public virtual double UplinkFrequencyLow {get; set;} |
| C++/CLI | |
|---|
public:
virtual property double UplinkFrequencyLow {
double get();
void set ( double value);
} |
Property Value
The default value is 1GHz.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 25.00
See Also