Keysight 89600 VSA .NET API
DownlinkSynchronizationSourceIndex Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > ComponentCarrier Class : DownlinkSynchronizationSourceIndex Property


Glossary Item Box

Gets or sets the index of the synchronization source used for this carrier if this carrier is downlink carrier.

Syntax

Visual Basic (Declaration) 
Public Overridable Property DownlinkSynchronizationSourceIndex As Integer
C# 
public virtual int DownlinkSynchronizationSourceIndex {get; set;}
C++/CLI 
public:
virtual property int DownlinkSynchronizationSourceIndex {
   int get();
   void set (    int value);
}

Property Value

The default value is 0

Remarks

This parameter is only used when the LinkDirection of this carrier is LinkDirection.Downlink. The first step of VSA 5G NR measurement is to use some known signal to identify the frame boundary, at the same time the coarse frequency offset is estimated. This process is called initial synchronization. For Downlink carrier, SSB or PDSCH-DMRS or PDCCH-DMRS can be used as the synchronization source. When SynchronizationSource.Auto is used, VSA automatically decides which source is used, the priority order is SSB first, then PDSCH-DMRS, and then PDCCH-DMRS. If there are multiple instances of the selected source type, the first one has higher priority, then the second and etc.. If SynchronizationSource.Auto is used, this parameter will not be used. If other SynchronizationSource is used, this value along with DownlinkSynchronizationSource decides which signal is used as the synchronization source. VSA will check whether the selected source is enabled in the signal configuration. If the selected source is not enabled, SynchronizationSource.Auto will be used and this parameter will not be used.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also