Keysight 89600 VSA .NET API
LteCrsRateMatchPatterns Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > ComponentCarrier Class : LteCrsRateMatchPatterns Property


Glossary Item Box

Gets a reference to the collection of LTE CRS Rate Match Patterns.

Syntax

Visual Basic (Declaration) 
Public Overridable ReadOnly Property LteCrsRateMatchPatterns As LteCrsRateMatchPatternCollection
C# 
public virtual LteCrsRateMatchPatternCollection LteCrsRateMatchPatterns {get;}
C++/CLI 
public:
virtual property LteCrsRateMatchPatternCollection^ LteCrsRateMatchPatterns {
   LteCrsRateMatchPatternCollection^ get();
}

Remarks

In 3GPP Rel15, only one LTE CRS rate match pattern is defined for each component carrier. As NR carrier bandwidth can be much wider than LTE bandwidth, in Rel16, it is possible that multiple LTE CRS rate match patterns are defined for one component carrier. For this reason, we define a collection for LTE CRS rate match pattern for each component carrier.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also