Keysight 89600 VSA .NET API
LteCrsRateMatchPattern Class
Members  See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : LteCrsRateMatchPattern Class


Glossary Item Box

Settings for LteCrsRateMatchPattern.

Syntax

Visual Basic (Declaration) 
Public MustInherit Class LteCrsRateMatchPattern 
   Inherits Agilent.SA.Vsa.RemotableObject
   Implements Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3 
C# 
public abstract class LteCrsRateMatchPattern : Agilent.SA.Vsa.RemotableObject, Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3  
C++/CLI 
public ref class LteCrsRateMatchPattern abstract : public Agilent.SA.Vsa.RemotableObject, Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3  

Remarks

settings for the RateMatchPatternLTE-CRS defined in 38.331. These settings are used to decide which subcarriers in which subframes are reserved for LTE CRS mapping.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also