| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property MaximumTransmissionBandwidth As MaximumTransmissionBandwidth | |
| C# | |
|---|---|
public abstract MaximumTransmissionBandwidth MaximumTransmissionBandwidth {get; set;} | |
| C++/CLI | |
|---|---|
public: abstract property MaximumTransmissionBandwidth MaximumTransmissionBandwidth { MaximumTransmissionBandwidth get(); void set ( MaximumTransmissionBandwidth value); } | |
Property Value
The default value is MaximumTransmissionBandwidth.FROne100MHzSetting this value reverts the per-subcarrier-spacing properties (ResourceGridCollection) to values defined in 3GPP specification 38.104 table 5.3.2-1 and 5.3.2-2. This value also determines the set of valid Numerology that can be used by a resource allocation within the carrier.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)