Keysight 89600 VSA .NET API
MimoResultsReferenceSignalIndex Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > ComponentCarrier Class : MimoResultsReferenceSignalIndex Property


Glossary Item Box

Gets or sets the index of the reference signal used for MIMO results calculation.

Syntax

Visual Basic (Declaration) 
Public Overridable Property MimoResultsReferenceSignalIndex As Integer
C# 
public virtual int MimoResultsReferenceSignalIndex {get; set;}
C++/CLI 
public:
virtual property int MimoResultsReferenceSignalIndex {
   int get();
   void set (    int value);
}

Property Value

The default value is 0

Remarks

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 30.00

See Also