| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property PdschReferenceGenerationMode As PdschReferenceGenerationMode | |
| C# | |
|---|---|
public virtual PdschReferenceGenerationMode PdschReferenceGenerationMode {get; set;} | |
| C++/CLI | |
|---|---|
public: virtual property PdschReferenceGenerationMode PdschReferenceGenerationMode { PdschReferenceGenerationMode get(); void set ( PdschReferenceGenerationMode value); } | |
Property Value
The default value is PdschReferenceGenerationMode.DemodBy default, the reference bits are based on the demodulated constellation points. When the signal is noisy or the modulation order is very high, there may be some detection error which causes inaccurate EVM measurement. For this kind of case, if the PDSCH bits are known, customer can specify the detection mode so a more accurate EVM can be calculated. For example, when the signal is Test Model signal, the PDSCH bits are PN23 sequence, which is reset at the frame start boundary with seeds of all zeros. PdschReferenceGenerationMode
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00