Keysight 89600 VSA .NET API
CsirsCdmType Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : CsirsCdmType Enumeration


Glossary Item Box

Enum values indicating the CSI-RS density in frequency domain.

Syntax

Visual Basic (Declaration) 
Public Enum CsirsCdmType 
   Inherits System.Enum
C# 
public enum CsirsCdmType : System.Enum 
C++/CLI 
public enum class CsirsCdmType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
Cdm2CDM Type FD-CDM2—
Cdm4CDM Type CDM4 (FD2,TD2)—
Cmd8CDM Type CDM8 (FD2, TD4)—
NoCdmCDM Type NO CDM—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20

See Also