Keysight 89600 VSA .NET API
Density Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Csirs Class : Density Property


Glossary Item Box

Gets or sets the CSI-RS density in frequency domain.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property Density As CsirsDensity
C# 
public abstract CsirsDensity Density {get; set;}
C++/CLI 
public:
abstract property CsirsDensity Density {
   CsirsDensity get();
   void set (    CsirsDensity value);
}

Property Value

The default , indicating no "Flexible" symbols should be allocated to this physical channel.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also