Keysight 89600 VSA .NET API
CsirsDensity Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : CsirsDensity Enumeration


Glossary Item Box

Enum values indicating the CSI-RS density in frequency domain.

Syntax

Visual Basic (Declaration) 
Public Enum CsirsDensity 
   Inherits System.Enum
C# 
public enum CsirsDensity : System.Enum 
C++/CLI 
public enum class CsirsDensity : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
Dot5EvenRBDensity is 0.5 and every even RB—
Dot5OddRBDensity is 0.5 and every odd RB—
OneRBDensity is 1—
ThreeRBDensity is 3—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20

See Also